EIO0000003565_05

Regular Cleaning

Cleaning This Product

NOTICE
EQUIPMENT DAMAGE
  • Power off this product before cleaning it.
  • Do not use hard or pointed objects to operate the touch panel.
  • Do not use paint thinner, organic solvents, or a strong acid compound to clean the unit.
Failure to follow these instructions can result in equipment damage.

When this product gets dirty, wipe this product with a soft, dry cloth or a soft cloth soaked in only water and wrung tightly.

NOTE: When the product is very dirty, soak the soft cloth in water with a neutral detergent, wring the cloth tightly and wipe the product while avoiding the product label.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.