EIO0000003565_05

Introduction

NOTICE
LOSS OF DATA
When using a SD Card:
  • Make sure you regularly back up the SD Card data.
  • While a SD Card is accessed, do not turn OFF or reset this product, and do not remove the SD Card.
  • Before removing the SD Card from this product, stop all operations on the SD Card.
  • Make sure of the SD Card’s orientation before inserting it into the SD Card slot.
Failure to follow these instructions can result in equipment damage.
NOTICE
LOSS OF DATA
When handling the SD Card:
  • Avoid storing the SD Card where there is static electricity or electromagnetic waves.
  • Avoid storing the SD Card in direct sunlight, near a heater, or other locations where high temperatures can occur.
  • Do not bend the SD Card.
  • Do not drop or strike the SD Card against another object.
  • Keep the SD Card dry.
  • Do not touch the SD Card connectors.
  • Do not disassemble or modify the SD Card.
  • Use the SD Card initialized by this product. You may not be able to use the SD Card initialized by other devices.
Failure to follow these instructions can result in equipment damage.
NOTE: To make your backups, you can either insert the SD Card directly into the SD Card Slot on your computer, or use a commercially available SD Card reader.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.