EIO0000003565_05

Removing from Display Module

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
Failure to follow these instructions will result in death or serious injury.
CAUTION
RISK OF INJURY
  • When removing the Box Module from the Display Module, hold the unit in place so it does not drop.
  • Use both hands.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
EQUIPMENT DAMAGE
When this product is mounted vertically, first remove the Display Module from the panel, then remove the Box Module from the Display Module.
Failure to follow these instructions can result in equipment damage.

Step

Action

1

When mounting this product vertically, remove the Display Module from the panel and place the Display Module on a clean and level surface with the screen facing down. Refer to Removing from the Panel.

2

Release the LOCK on the top of the Box Module as illustrated.

1 LOCK

2 Display Module

3

Lift the Box Module in the direction indicated by arrow (A) in the diagram and remove it by sliding in the direction indicated by arrow (B).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.