EIO0000003565_05

Installing onto Display Module

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
Failure to follow these instructions will result in death or serious injury.
NOTICE
EQUIPMENT DAMAGE
  • When mounting this product vertically, before attaching to the panel, install the Box Module onto the Display Module.
  • When installing the Box Module onto the Display Module, place the Display Module on a clean and level surface with the screen facing downward.
Failure to follow these instructions can result in equipment damage.

Step

Action

1

Pull the LOCK forward on the top of the Box Module to release the lock as illustrated.

1 LOCK

2

Insert the protruding points on the bottom left and right of the Box Module into the two holes on the back of the Display Module to attach the Box Module.

2 Protruding points

3 Box Module

4 Holes for insertion

5 Display Module

3

Fully push on the LOCK on the top of the Box Module to mount the Box Module on the Display Module

1 LOCK

NOTE: For instructions on how to mount the Display Module to the panel, refer to Installing to the Panel.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.