EIO0000003565_05

Panel Cut Dimensions

Based on the panel cut dimensions, open a mount hole on the panel.

Model Name

A

B

C

HMIDT35X

190 mm (+1/-0 mm)

(7.48 in [+0.04/-0 in])

135 mm (+1/-0 mm)

(5.31 in [+0.04/-0 in])

1.6...5 mm (0.06...0.2 in)

HMIDT65X

295 mm (+1/-0 mm)

(11.61 in [+0.04/-0 in])

217 mm (+1/-0 mm)

(8.54 in [+0.04/-0 in])

1.6...5 mm (0.06...0.2 in)

HMIDT75X

394 mm (+1/-0 mm)

(15.51 in [+0.04/-0 in])

250 mm (+1/-0 mm)

(9.84 in [+0.04/-0 in])

1.6...5 mm (0.06...0.2 in)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.