EIO0000003565_05

System Design

Box Module

*1 In order to use this as an isolation port, Isolation Unit is required. To use RS-232C isolation unit, set the #9 pin of the COM port to VCC. (Only for COM2)

*2 Refer to Accessories.

*3 For information on how to connect controllers and other types of equipment, refer to the corresponding device driver manual of your screen editing software.

*4 For supported models, contact your local Schneider Electric support representative.

*5 Connects only to eXtreme Display. Refer to the Part Numbers.

Display Module

*1 Connects only to eXtreme Box.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.