EIO0000003565_05

HMIG3X

Side

HMIG3X

Front

Right

Bottom

Rear

A: Auxiliary output/ Speaker output interface (AUX)

This interface is alarm output or buzzer output, and sound output.

B: Status LED*1

C: Card access LED*1

D: USB (mini-B) interface*2

E: Expansion unit interface cover (EXT)*3

The expansion unit can be embedded in the expansion unit interface cover opening, and battery for memory backup can be connected or replaced.

F: Storage card cover

G: System card cover

You cannot open this cover when the Box Module is in operation.

H: USB (Type A) interface*2

I: Ethernet interface (Ethernet1)*2

J: Ethernet interface (Ethernet2)*2

K: COM1 LED*2

L: Serial interface (COM1)*2

M: Serial interface (COM2)*2

N: Display Module interface

CAUTION
RISK OF BURNING INJURY
Do not connect the Modbus RJ-45 communication cable to the Ethernet interface.
Failure to follow these instructions can result in injury or equipment damage.

*1 Refer to LED Indications

*2 Refer to Interface Specifications

*3 Refer to Replacing the Primary Battery

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.