EIO0000003565_05

Serial Interface (RS-485 [Isolation]) for COM1

Introduction

NOTE: For information on how to connect controllers and other types of equipment, refer to the corresponding device driver manual of your screen editing software.
CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
  • Use a RJ-45 connector that has a functional locking tab.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Use within the rated current.

RS-485 (Isolation)

RJ-45 connector

NOTE: When setting up RS-485 communication, the cable diagram for some equipment may require polarization on the terminal side. Change the setting for polarization with your screen editing software.

Product side

Pin No.

RS-485 (Isolation)

Signal name

Direction

Meaning

1

NC

No connection

2

NC

No connection

3

NC

No connection

4

Line A

Input/Output

Transfer Data A (+)

5

Line B

Input/Output

Transfer Data B (-)

6

RS (RTS)

Output

Request to Send

7

NC

No connection

8

SG

Signal Ground

Shell

FG

Functional Ground

NOTE: The FG and SG terminals are isolated.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.