AUX Connector
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Step |
Action |
---|---|
1 |
Align the flat-head screwdriver with the groove of the orange spring release button, and while depressing the button insert the electric wire into the wire insertion slot (round-shaped hole). |
2 |
Pull out the screwdriver from the release button. The wire insertion slot is then closed and the wire is held securely in place. To remove the wire, align the flat-head screwdriver with the groove of the release button, and while depressing the button pull the wire out. |
3 |
Insert the wired AUX connector into the Auxiliary Output/Speaker Output Interface (AUX) of this product. |
Recommendations:
-
AUX Connector: HMIZGAUX by Schneider Electric
-
Screwdriver: Be sure the screwdriver has the following dimensions:
- Blade thickness: 0.4 mm (0.02 in)
- Blade width: 2.0 mm (0.08 in)
Point shape should have isolation properties meeting DIN 5264 and EN60900.
-
Wire should be AWG 28 to AWG 20 thick and twisted.
-
Applicable wire sizes are Style 1015 and Style 1007.
-
Be sure to strip 8.0 mm (0.31 in) of cover from the wire.
-
Use copper wire rated for 75 °C (167 °F) or higher.