EIO0000004129.03

Federal Communication Commission Radio Frequency Interference Statement - For USA

FCC Radio Interference Information

This product has been tested and found to comply with the Federal Communications Commission (FCC) limits for a Class A digital device, pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a commercial, industrial or business environment. This product generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause or be subject to interference with radio communications. To minimize the possibility of electromagnetic interference in your application, observe the following two rules:

  • Install and operate this product in such a manner that it does not radiate sufficient electromagnetic energy to cause interference in nearby devices.

  • Install and test this product to ensure that the electromagnetic energy generated by nearby devices does not interfere with the operation of this product.

WARNING
ELECTROMAGNETIC / RADIO INTERFERENCE, UNINTENDED EQUIPMENT OPERATION
Check for electromagnetic and radio interference. If interference is detected, take the following actions.
  • Increase the distance between this product and the interfering equipment.
  • Reorient this product and the interfering equipment.
  • Reroute power and communication lines to this product and the interfering equipment.
  • Connect this product and the interfering equipment to different power supplies.
  • Always use shielded cables when connecting this product to a peripheral device or another computer.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Changes or modifications not expressly approved by the party responsible for compliance could void the user's authority to operate this product.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.