EIO0000004129.03

Specifications of Each Interface

Serial interface COM1
Asynchronous transmission RS-232C/485
Data length 7 or 8 bits
Stop bit 1 or 2 bits
Parity None, odd, or even
Data transmission speed 2,400...115,200 bps, 187,500 bps (MPI)
Connector Modular jack (RJ-45)
USB (Type A) interface
Connector USB 2.0 (Type A) x 1
Power supply voltage 5 Vdc ±5%
Maximum current supplied 500 mA
Maximum transmission distance 5 m (16.4 ft)
USB (micro-B) interface
Connector USB 2.0 (micro-B) x 1
Maximum transmission distance 5 m (16.4 ft)
Ethernet interface
Standard IEEE802.3i/IEEE802.3u, 10BASE-T/100BASE-TX
Connector Modular jack (RJ-45) x 2
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.