EIO0000004129.03

Part Numbers

Part Number List

Series Model name Part number
Harmony STM6 HMISTM6200 HMISTM6200
HMISTM6400 HMISTM6400
HMISTM6BOX HMISTM6BOX
HMISTM6BOXIOT HMISTM6BOXIOT
NOTE: All part numbers may be followed by any letter or number.

Part Number Configuration

The following describes the configuration of part numbers.

Digit position
1 2 3 4 5 6 7 8 9 10 11 and later
  (model) (series) (display size) (type) (available software and others)
HMI STM 6 2: 4"
4: 7"
00: Standard -
BOX: No display -: EcoStruxure Operator Terminal Expert
IOT: EcoStruxure Machine Scada Expert
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.