EIO0000004129.03

Electrical Specifications

Rear Module

Rated input voltage 24 Vdc
Input voltage limits 19.2...28.8 Vdc
Voltage dip/short interruption immunity 5 ms or less (at rated input voltage)
Power consumption Max 6.8 W
When power is not supplied to external devices 3.5 W
In-rush current 30 A or less
Noise immunity Noise voltage: 1,000 Vp-p
Pulse duration: 1 μs
Rise time: 1 ns (via noise simulator)
Dielectric strength 1,000 Vac for 1 minute (between power terminal and FG terminal)
Insulation resistance 500 Vdc, 10 MΩ or more (between power terminal and FG terminals)

Display Module

Specification HMISTM6200 HMISTM6400
Power consumption Max 1.0 W 3.6 W
When screen turns off the backlight (standby mode) 0.6 W 1.3 W
NOTE: The power consumption for the combined unit of the rear module and the display module equals the sum of power consumption of the two modules.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.