EIO0000004129.03

Replacing the Installation Gasket

The installation gasket provides protection against dust and moisture.
The gasket must be inserted correctly into the groove for moisture resistance for the display module.

NOTICE
EQUIPMENT DAMAGE
  • Inspect the gasket periodically as required by your operating environment.
  • Replace the gasket at least once a year, or as soon as scratches or dirt become visible.
  • Be careful not to stretch the gasket unnecessarily.
Failure to follow these instructions can result in equipment damage.
  1. Place the display module on a flat, level surface, with the display face pointing down.
  2. Remove the gasket from the display module.
  3. Attach the new gasket to the display module.
    1. Installation gasket

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.