EIO0000004129.03

Structural Specifications

Rear Module

Grounding Functional grounding: Grounding resistance of 100 Ω or less, 2 mm2 (AWG 14) or thicker wire, or your country's applicable standard (SG and FG are connected inside the product).
Cooling method Natural air circulation
Structure IP20
External dimensions (W x H x D) 145.6 x 108.23 x 41.4 mm (5.73 x 4.26 x 1.63 in) (excluding protrusions)
Weight 0.27 kg (0.6 lb) or less
NOTICE
EQUIPMENT DAMAGE
  • Operate and store this product in areas where temperatures are within the product's specifications.
  • Do not restrict or block the product's ventilation slots.
Failure to follow these instructions can result in equipment damage.

Display Module

  HMISTM6200 HMISTM6400
Cooling method Natural air circulation
Structure*1 IP65F, UL 50/50E, Type 1, Type 4X (indoor use only), Type 12, Type 13
External dimensions (W x H x D) 140.4 x 101.1 x 13.9 mm
(5.53 x 3.98 x 0.55 in) (excluding protrusions)
201.2 x 137.2 x 17.1 mm
(7.92 x 5.4 x 0.67 in) (excluding protrusions)
Panel cutout dimensions Diameter 22.5 mm (0.88 in)
Weight 0.22 kg (0.49 lb) or less 0.49 kg (1.08 lb) or less

*1 The front of this product has been tested to comply with the specified standards when installed in a solid panel. However, it is not intended for use in all environments. In environments where the product is exposed to liquids (including jets and sprays) for extended periods, there is a risk that liquids may enter the product due to causes such as peeling of the protective sheet or damage to the front glass cover. In such environments, implement appropriate protective measures based on the specific conditions. Therefore, prior to installing this product, be sure to confirm the type of conditions that will be present in this product's operating environment.

If the installation gasket is used for a long period of time, or if this product and its gasket are removed from the panel, the original level of protection cannot be kept. To maintain the original protection level, be sure to replace the installation gasket regularly.

NOTE: IP65F is not part of UL certification.
NOTICE
EQUIPMENT DAMAGE
  • Ensure this product is not in permanent and direct contact with oils.
  • Do not press on the display of this product with excessive force or with a hard object.
  • Do not press on the touch panel with a pointed object, such as the tip of a mechanical pencil or a screwdriver.
  • Do not expose the product to direct sunlight.
  • Operate and store this product in areas where temperatures are within the product's specifications.
Failure to follow these instructions can result in equipment damage.
NOTICE
EQUIPMENT DAMAGE
  • Inspect the gasket periodically as required by your operating environment.
  • Replace the gasket at least once a year, or as soon as scratches or dirt become visible.
Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.