EIO0000004129.03

LED Indications

Status LED

After power is turned on, normal status indication by the LED is: red light > flashing orange > green light.

Color Indicator HMI operation
Green ON In operation
Flashing once every 5 seconds*1 Backlight OFF (Standby Mode)
Orange Flashing Software starting up
Red ON Power is ON.
- OFF Power is OFF.

*1 Only models supported by screen editing software "EcoStruxure Operator Terminal Expert". On models supported by other software, the LED light remains green even if the product's backlight is off (Standby Mode).

For other LED indications, refer to the manual of your screen editing software.

Ethernet LED

Color Indicator Description
Green (Link) ON Data transmission is available.
OFF No connection or error
Green (Active) Flashing Data transmission is occurring.
OFF No data transmission
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.