EIO0000004129.03

Precautions for Building into an End-use Product

The display module of this product is designed for use on flat surfaces of IP65F, UL 50/50E, Type 1, Type 4X (indoor use only), Type 12 and Type 13 enclosures.

Be aware of the following when building this product into an end-use product:

  • The rear module of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product's overall enclosure.

  • The rear module of this product is an open-type device and is meant to be installed in an enclosure suitable for the environment. Install in an enclosure where the equipment is inaccessible without the use of tools.

  • Install this product in an enclosure with mechanical rigidity.

  • This product is not designed for outdoor use. UL certification obtained is for indoor use only.

  • Install and operate the display module with its front panel facing outward.

NOTE: IP65F is not part of the UL certification.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.