EIO0000004129.03

Precautions for Installing to an End-use Product

Be aware of the following when installing this product to an end-use product:

  • This product is an open-type device and is meant to be installed in an enclosure suitable for the environment. Install in an enclosure where the equipment is inaccessible without the use of tools.

  • Install this product in an enclosure with mechanical rigidity.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.