EIO0000004129.03

Memory

System memory*1 Flash EPROM 1 GB (operating system, project data, and other data)
Backup memory*1*2 NVRAM 512 KB

*1 For the usage capacity of each memory depends on your screen editing software.

*2 For HMISTM6BOXIOT, the backup memory is not used.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.