EIO0000004129.03

Removal Procedure from DIN Rail

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
Failure to follow these instructions will result in death or serious injury.
  1. Push and hold the button at the top of the rear module, and pull the rear module straight out.
  2. Push down on the rear module installation adapter and unhook the bottom part of the adapter from the DIN rail.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.