EIO0000004129.03

Power Supply Precautions

DANGER
SHORT CIRCUIT, FIRE, OR UNINTENDED EQUIPMENT OPERATION
  • Install and fasten this product in an installation panel or cabinet prior to connecting power supply and communication lines.
  • Securely attach power cables to an installation panel or cabinet.
  • Avoid excessive force on the power cable.
Failure to follow these instructions will result in death or serious injury.

Improving Noise/Surge Resistance

  • This product's power cord should not be bundled with or kept close to main circuit lines (high voltage, high current), power lines, or input/output lines, and their various systems should be kept separate. When power lines cannot be wired via a separate system, use shielded cables for input/output lines.

  • Make the power cord as short as possible, and be sure to twist the ends of the wires together (i.e. twisted pair cabling) from close to the power supply unit.

  • If there is an excess amount of noise on the power supply line, connect a noise reducing transformer, noise filter, or other before turning on the power.

  • Connect a surge protection device to handle power surges.

  • To increase noise resistance, attach a ferrite core to the power cable.

Power Supply Connections

  • Use UL Listed power source with LPS (Limited Power Source) or Class 2 output.

  • If the voltage variation is outside the prescribed range, connect a regulated power supply.

    1. Regulated power supply

    2. Twisted-pair cord

    3. This product

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.