EIO0000004129.03

Installation Procedure

This section describes how to install the rear module and display module to the panel.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
  • Use only the specified voltage when operating this product. This product is designed to use 24 Vdc. Always check whether your device is DC powered before applying power.
  • When using this product in Class I, Division 2, Groups A, B, C, and D hazardous locations, install this product in an enclosure that prevents the operator from touching the back of this product without the use of tools.
Failure to follow these instructions will result in death or serious injury.
NOTICE
EQUIPMENT DAMAGE
Always use the installation gasket.
Failure to follow these instructions can result in equipment damage.
  1. Place the display module on a clean and level surface with the screen facing down.
  2. Check that the gasket is seated securely into the bezel groove, which runs around the perimeter of the display panel frame.
    NOTE: Always use the installation gasket, since it absorbs vibration in addition to repelling water. For the procedure on replacing the installation gasket, refer to Replacing the Installation Gasket.
  3. Based on this product's Panel Cutout Dimensions, open a mount-hole on the panel.
  4. Insert the display module and the anti-rotation tee into the panel hole from the front side. Use the socket wrench to tighten the nut. The necessary torque for the nut is 1.2 to 2.0 N•m (10.62 to 17.70 lb-in).
    NOTE:
    • The anti-rotation tee is used to install the display module horizontally on the panel. When you do not use an anti-rotation tee, applying 2.5 N•m (22.12 lb-in) or more force to the display module could cause the product to rotate. By using an anti-rotation tee, 6 N•m (53.10 lb-in) or more force could cause the product to rotate.

    • If the panel thickness does not meet the specified conditions, use the spacer (sold separately).

    1. Display module

    2. Panel

    3. Installation nut

    4. Anti-rotation tee

    5. Socket wrench

  5. If the panel thickness is 3.8 mm (0.15 in) or less, push in the bumper on the rear module until you hear a click. If the panel thickness is more than 3.8 mm (0.15 in), do not change the bumper position.
    NOTE: To return the bumper to its original position, use a screwdriver or other tool as a lever to push the bumper up.
  6. Insert and push the rear module straight in to the display module, until they lock into place.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.