EIO0000004129.03

Rear Module Installation Adapter External Dimensions

Rear Module Installation Adapter Dimensions

  1. Front

  2. Right

  3. Bottom

  4. Rear

Dimensions with Separation Cable Attached

  1. Front

  2. Right

*1 To assemble this product, you need 20 mm (0.78 in) or more space to bend the rubber portion at the end of the cable.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.