EIO0000004129.03

Attaching USB Clamp mini-B

When using the USB micro-B cable (option), you can use the USB mini-B clamp included in the Accessory kit (sold separately) to prevent the cable from being disconnected.

WARNING
EXPLOSION HAZARD
  • Verify the power, input, and output (I/O) wiring are in accordance with Class I, Division 2 wiring methods.
  • Substitution of any components may impair suitability for Class I, Division 2.
  • Confirm that the USB cable has been fixed with the USB clamp before using the USB interface.
  • Remove power before attaching or detaching any connectors to or from this product.
  • Use the USB (micro-B) interface for temporary connection only during maintenance and setup of the device.
  • Do not use the USB (micro-B) interface in hazardous locations.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Insert the USB cable into the USB (micro-B) interface.
    1. USB interface

  2. Attach the USB clamp to fix the USB cable in place. Insert the USB holder into the USB (micro-B) interface.

    B. USB clamp

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.