EIO0000004129.03

Serial Interface

The serial interface is not isolated. The SG (signal ground) and FG (frame ground) terminals are connected inside this product.

You can switch the communication method between RS-232C and RS-485 via the software.

NOTE: For information on how to connect controllers and other types of equipment, refer to the corresponding device driver manual of your screen editing software.
DANGER
ELECTRIC SHOCK AND FIRE
When using the SG terminal to connect an external device to this product:
  • Verify that a ground loop is not created when you set up the system.
  • Connect the SG terminal to remote equipment when the external device is not isolated.
  • Connect the SG to a known reliable ground connection to reduce the risk of damaging the circuit.
Failure to follow these instructions will result in death or serious injury.
CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
  • Use a RJ-45 connector that has a functional locking tab.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Use within the rated current.

RS-232C/RS-485

RJ45 connector

NOTE: When setting up RS-485 communication, the cable diagram for some equipment may require polarization on the terminal side. Change the setting for polarization with your screen editing software.
Pin No. RS-232C/RS-485
Signal name Direction Description
1 RD (RXD) Input Receive Data (RS-232C)
2 SD (TXD) Output Send Data (RS-232C)
3 NC - No connection
4 D1 Input/Output Transfer Data (RS-485)
5 D0 Input/Output Transfer Data (RS-485)
6 RS (RTS) Output Request To Send
7 NC - No connection
8 SG - Signal Ground
Shell FG - Frame Ground
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.