EIO0000004129.03

Parts Identification

Parts Identification (Display Module)

Front
  1. Status LED

Parts Identification (Rear Module)

Front
Bottom
  1. Status LED

  2. Bumper

  3. USB (Type A) interface

  4. USB (micro-B) interface

  5. Power plug connector

  6. Serial interface (COM1)

  7. Ethernet interface (ETH1)

  8. Ethernet interface (ETH2)

WARNING
UNINTENDED EQUIPMENT OPERATION
  • Do not connect the product to the computer with the USB (micro-B) cable unless the product is powered by the power cable.
  • Remove the USB (micro-B) cable before communicating with the host controller and other types of equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.