EIO0000004129.03

System Design

This section describes the system configuration with this product and peripheral equipment.

NOTE:
  • To use the rear module, connect the display module or rear module installation adapter.

  • When using HMISTM6BOXIOT, connect it to the rear module mounting adapter. It cannot be connected to the display module.

*1 Refer to Accessories.

*2 For information on how to connect controllers and other types of equipment, refer to the corresponding device driver manual of your screen editing software.

*3 For supported models, contact your local Schneider Electric support representative.

To use this product, transferring project data from the screen editing software is required. For details about transfer, refer to the software manual.
When transferring using the USB (micro-B) interface, connect cables in the following order:

  1. Attach the transfer cable to the USB (micro-B) interface of this product.

  2. Attach the power cable to this product, then connect the power cable to an external power source.

  3. Connect the transfer cable to the computer.

WARNING
UNINTENDED EQUIPMENT OPERATION
  • Do not connect the product to the computer with the USB (micro-B) cable unless the product is powered by the power cable.
  • Remove the USB (micro-B) cable before communicating with the host controller and other types of equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

When using HMISTM6BOXIOT, you need to make initial settings before transferring the project data for the first time. For how to set up the product, refer to EcoStruxure Machine SCADA Expert HMI Runtime Reference Manual (EIO0000004669).
You can download the manuals related to this product from our website.
www.se.com

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.