EIO0000004129.03

Removal Procedure

This section describes how to remove the rear module and display module from the panel.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
Failure to follow these instructions will result in death or serious injury.
NOTICE
EQUIPMENT DAMAGE
Be sure to remove the rear module from the display module without twisting.
Failure to follow these instructions can result in equipment damage.
  1. Push and hold the button at the top of the rear module, and pull the rear module straight out.
  2. Remove the nut and the display module from the panel.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.