Application 2: Breaker Operation
Presentation
The application is used to control the opening and closing of the device.
The application takes into account:
-
Control mode selection (local or remote), defined by the control mode selector switch wired on a digital input.
NOTE: When IO module is used with application 2 Breaker operation, the control mode of the device (local or remote) is defined only by the control mode selector switch wired on a digital input of the IO module, and cannot be changed by a remote controller using the communication network or by the FDM121 display.
-
Local opening and closing orders issued from:
-
Local push-buttons wired on digital inputs.
-
Local FDM121 display.
-
-
Remote opening and closing orders issued from:
-
Remote PLC outputs wired on digital inputs.
-
Remote controller using the communication network.
-
IFE or EIFE webpages.
-
-
COM and IO inhibit close order issued from:
-
Local selector switch wired on a digital input.
-
Remote controller using the communication network.
WARNINGRESTRICTED CLOSING INHIBITIONDo not use the inhibit close order to lock the device in open position.Failure to follow these instructions can result in death, serious injury, or equipment damage. -
The inhibit close order inhibits only the close orders issued from the IO module, FDM121 display, and a remote controller. The close orders issued from the front-face-button, BPFE, or from push-button directly connected to XF voltage release are not inhibited.
The close order can be inhibited either by a local command from the IO module or by a remote command from the remote controller.
After the close order has been inhibited locally, it has to be enabled by the local command from the IO module.
After the close order has been inhibited remotely, it has to be enabled by the remote command from the remote controller.
After the close order has been inhibited locally and remotely, it has to be enabled by the local command from the IO module and by the remote command from the remote controller.
The remote control orders issued from a remote controller using the communication network requires a communication interface module (IFM, IFE, or EIFE interface):
-
MasterPacT MTZ circuit breakers are controlled remotely by MicroLogic X commands, refer to the MasterPacT MTZ Modbus Communication Guide.
-
MasterPacT NT/NW and ComPacT NS or PowerPacT P- and R-frame circuit breakers are controlled remotely by BCM ULP module commands. For more information, refer to the following user guides in Related Documents:
-
MasterPacT NT/NW Modbus Communication Guide
-
ComPacT NS Modbus Communication Guide
-
MasterPacT NT/NW and PowerPacT P- and R-Frame Modbus Communication Guide
-
-
ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breakers are controlled remotely by BSCM or BSCM Modbus SL/ULP module commands. For more information, refer to the following user guides in Related Documents:
- ComPacT NSX Modbus Communication Guide
-
PowerPacT H-, J-, and L-Frame Modbus Communication Guide
Compatible Devices
|
Range |
Minimum Hardware Configuration Required |
|---|---|
|
MasterPacT MTZ circuit breaker |
|
|
|
|
|
Input/Output Assignment
|
Input |
Assignment |
|---|---|
|
I1 |
Local(0) or Remote(1) control mode. If the input is not wired, the IMU is in local mode (I1=0). If there is a control mode selector switch, it is recommended to wire I1 to have I1=1. |
|
I2 |
Remote open order |
|
I3 |
Remote close order |
|
I4 |
Inhibit(0) or Enable(1) close order. If the input is not wired, close order is inhibited (I4=0). |
|
I5 |
Local open order |
|
I6 |
Local close order |
|
Output |
Assignment |
|---|---|
|
O1 |
Local control mode |
|
O2 |
Inhibit close order activated by IO module |
|
O3 |
Available |
Wiring Diagram with MasterPacT MTZ Circuit Breaker
Wiring Diagram with MasterPacT NT/NW and ComPacT NS 630b-1600 or PowerPacT P-Frame Circuit Breaker
Wiring Diagram with ComPacT NSX or PowerPacT H-, J-, and L-Frame Circuit Breaker
Device Open Command
|
I1 |
Local(0) or Remote(1) control mode |
|
I2 |
Remote open order |
|
I5 |
Local open order |
|
FDM121 open |
Open order from local FDM121 display |
|
COM open |
Open order from a remote controller using the communication network |
|
Open |
Device open command to:
|
MasterPacT MTZ, MasterPacT NT/NW, and ComPacT NS 630b-1600 or PowerPacT P-Frame Circuit Breakers Direct Open Order
On MasterPacT MTZ, MasterPacT NT/NW, and ComPacT NS 630b-1600 or PowerPacT P-frame circuit breakers, an open order command can be wired directly to the MX communicating voltage releases to open the device, without taking into account the control mode or the data processed by the IO module.
Inhibit Close Order
|
I4 |
Inhibit(0) or Enable(1) close order |
|
COM inhibit close |
Inhibit close order from a remote controller using the communication network |
|
COM enable close |
Enable close order from a remote controller using the communication network |
|
Inhibit close |
Close order is inhibited(1) or enabled(0) |
Device Close Command
|
Inhibit close |
Close order inhibited(1) or enabled(0) |
|
I1 |
Local(0) or Remote(1) control mode |
|
I3 |
Remote close order |
|
I6 |
Local close order |
|
FDM121 close |
Close order from the local FDM121 display |
|
COM close |
Close order from a remote controller using the communication network |
|
Close |
Device close command to:
|
MasterPacT MTZ, MasterPacT NT/NW, and ComPacT NS 630b-1600 or PowerPacT P-Frame Circuit Breakers Direct Close Order
On MasterPacT MTZ, MasterPacT NT/NW and ComPacT NS 630b-1600 or PowerPacT P-frame circuit breakers, a direct close order can be wired directly to the XF communicating voltage release to close the devices.
This close order:
-
Is not inhibited by the close inhibit order.
-
Does not take into account the control mode or the data processed by IO module.