Application 4: Light and Load Control
Presentation
-
The light-control application is used to switch the lights on and off remotely. The lights are controlled by an impulse relay. The switch order can be either delayed or not.
-
The load-control application is used to switch the loads on and off remotely. The loads are controlled by a contactor. The switch order can be either delayed or not.
The light and load orders are issued from:
-
The local FDM121 display.
-
The local push-buttons (S1, S2...) connected to the impulse relay (light control).
-
A remote controller using the communication network.
-
The IFE or EIFE webpages, only when the IO module is connected to a circuit breaker.
The orders issued from a remote controller using the communication network correspond to IO module commands. These orders require a communication interface module (IFM, IFE, or EIFE interface).
Input/Output Assignment
|
Input |
Assignment |
|---|---|
|
I1 |
Lighting pulse relay feedback |
|
I2 |
Load contactor feedback |
|
I3, I4, I5, I6 |
Available |
|
Output |
Assignment |
|---|---|
|
O1 |
Lighting pulse relay command |
|
O2 |
Load contactor command |
|
O3 |
Available |
Wiring Diagram
Light Control Block Diagram
The light is controlled by an impulse relay. The relay is switched off and on after receiving a command pulse delivered by the IO module or local push-buttons.
The delayed switching order specifies the waiting time in seconds before execution of the order by the IO module.
|
I1 |
Lighting impulse relay feedback |
|
FDM121 light on |
Instantaneous light switch on order from the FDM121 display |
|
COM light on |
Instantaneous light switch on order from a remote controller using the communication network |
|
COM light on/t |
Delayed light switch on order with t seconds delay from a remote controller using the communication network |
|
FDM121 light off |
Instantaneous light switch off order from the FDM121 display |
|
COM light off |
Instantaneous light switch off order from a remote controller using the communication network |
|
COM light off/t |
Delayed light switch off order with t seconds delay from a remote controller using the communication network |
|
O1 |
Lighting impulse relay command |
Load Control Block Diagram
The load is controlled by a contactor. The contactor is switched on and off by the IO module. The delayed switching order specifies the waiting time in seconds before execution of the order by the IO module.
|
I2 |
Load contactor feedback |
|
FDM121 load on |
Instantaneous load switch on order from the FDM121 display |
|
COM load on |
Instantaneous load switch on order from a remote controller using the communication network |
|
COM load on/t |
Delayed load switch on order with t seconds delay from a remote controller using the communication network |
|
FDM121 load off |
Instantaneous load switch off order from the FDM121 display |
|
COM load off |
Instantaneous load switch off order from a remote controller using the communication network |
|
COM load off/t |
Delayed load switch off order with t seconds delay from a remote controller using the communication network |
|
O2 |
Load contactor command |
Application Events
The following events are generated by the application. For more information on IO module events, refer to Events and Alarms.
|
Code |
Description |
Type |
Priority |
Reset |
|---|---|---|---|---|
|
2560 (0x0A00) |
Aux contact of the load contactor 1 is not closed |
Alarm |
Medium |
Manual or remote |
|
2561 (0x0A01) |
Aux contact of the load contactor 1 is not opened |
Alarm |
Medium |
Manual or remote |
Recommended action: Check operation of the load and the inputs/outputs of the IO module.