System Events
List of System Events
The following events are generated by IO module 1 or IO module 2.
|
Code IO1 |
Code IO2 |
Description |
Type |
Priority |
Reset |
|---|---|---|---|---|---|
|
1537 (0x0601) |
1793 (0x0701) |
Watchdog reset |
Event |
N/A |
N/A |
|
1539 (0x0603) |
1795 (0x0703) |
IO module in STOP mode |
Alarm |
High |
Manual or remote |
|
1540 (0x0604) |
1796 (0x0704) |
IO module in ERROR mode |
Alarm |
Medium |
Manual or remote |
|
1541 (0x0605) |
1797 (0x0705) |
Application rotary switch position change |
Event |
N/A |
N/A |
|
1542 (0x0606) |
1798 (0x0706) |
Setting locking pad rotary switch position change |
Event |
N/A |
N/A |
|
1543 (0x0607) |
1799 (0x0707) |
Source address DIP switch position change |
Event |
N/A |
N/A |
|
3328 (0x0D00) |
3328 (0x0D00) |
Critical hardware modules discrepancy |
Alarm |
High |
Auto |
|
3329 (0x0D01) |
3329 (0x0D01) |
Critical firmware modules discrepancy |
Alarm |
High |
Auto |
|
3330 (0x0D02) |
3330 (0x0D02) |
Non-critical hardware modules discrepancy |
Alarm |
Medium |
Auto |
|
3331 (0x0D03) |
3331 (0x0D03) |
Non-critical firmware modules discrepancy |
Alarm |
Medium |
Auto |
Watchdog Reset
The watchdog reset is a firmware reset where the IO module restarts itself after detection of an IO module processing time-out.
IO Module in STOP Mode
The IO module in STOP mode alarm is generated when the IO module is out of service. Replace the IO module.
IO Module in ERROR Mode
IO module in ERROR mode alarm is generated when the IO module detects that the EEPROM memory is corrupted. Replace the IO module at the next maintenance operation.
Application Rotary Switch Position Change
The application rotary switch is located on the front face of the IO module. Each time the position of the application rotary switch is changed from one application to another application, an event is generated.
Setting Locking Pad Rotary Switch Position Change
The setting locking pad is located on the front face of the IO module. Each time the position of the setting locking pad is changed, an event is generated.
Source Address DIP Switch Position Change
The source address DIP switch is located on the bottom of the IO module. Each time the position of the DIP switch is changed, an event is generated.
Critical Hardware Modules Discrepancy
The IO module detects a hardware discrepancy between the modules of the IMU that requires an immediate action. Use the EcoStruxure Power Commission software to check the hardware compatibility of the IMU modules and follow the recommended actions.
Critical Firmware Modules Discrepancy
The IO module detects a firmware discrepancy between the modules of the IMU that requires an immediate action. Use the EcoStruxure Power Commission software to check the firmware compatibility of the IMU modules and follow the recommended actions. If required, update module firmware.
Non-Critical Hardware Modules Discrepancy
The IO module detects a hardware discrepancy between the modules of the IMU that requires a non-urgent action. Use the EcoStruxure Power Commission software to check the hardware compatibility of the IMU modules and follow the recommended actions.
Non-Critical Firmware Modules Discrepancy
The IO module detects a firmware discrepancy between the modules of the IMU that requires a non-urgent action. Use the EcoStruxure Power Commission software to check the firmware compatibility of the IMU modules and follow the recommended actions. If required, update module firmware.