Threshold Overrun of Input Counter Indicator
Presentation
The input counter threshold overrun event can be assigned to the digital outputs for local indication. The input counter threshold overrun output can be configured using the EcoStruxure Power Commission software.
Input/Output Assignment
The table below lists the possible assignment of the digital outputs, according to the predefined application selected on the IO module:
|
Outputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
IO1 input I1 counter overrun to input I6 counter overrun |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
IO2 input I1 counter overrun to input I6 counter overrun |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |