User-Defined Input Acquisition
Presentation
The IO module can acquire user-defined indications delivered by external devices through digital inputs. The status of the input is displayed on the FDM121 display. The indication description can be entered using the EcoStruxure Power Commission software.
Each change of state of a user-defined input generates an event. For more information on the IO module events, refer to Events and Alarms.
|
Code IO1 |
Code IO2 |
Description |
Type |
Priority |
Reset |
|---|---|---|---|---|---|
|
1579 (0x062B) |
1835 (0x072B) |
User-defined input 1 |
Alarm |
Medium |
Manual or remote |
|
1580 (0x062C) |
1836 (0x072C) |
User-defined input 2 |
Alarm |
Medium |
Manual or remote |
|
1581 (0x062D) |
1837 (0x072D) |
User-defined input 3 |
Alarm |
Medium |
Manual or remote |
|
1582 (0x062E) |
1838 (0x072E) |
User-defined input 4 |
Alarm |
Medium |
Manual or remote |
|
1583 (0x062F) |
1839 (0x072F) |
User-defined input 5 |
Alarm |
Medium |
Manual or remote |
|
1584 (0x0630) |
1840 (0x0730) |
User-defined input 6 |
Alarm |
Medium |
Manual or remote |
Input/Output Assignment
The table below lists the possible assignment of the digital inputs, according to the predefined application selected on the IO module:
|
Inputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
User-defined input 1 |
– |
– |
– |
– |
– |
– |
– |
– |
I1 |
|
User-defined input 2 |
– |
– |
– |
– |
– |
– |
– |
– |
I2 |
|
User-defined input 3 |
– |
– |
– |
I3 |
– |
– |
– |
– |
I3 |
|
User-defined input 4 |
I4 |
– |
– |
I4 |
– |
– |
– |
– |
I4 |
|
User-defined input 5 |
I5 |
– |
– |
I5 |
– |
– |
– |
– |
I5 |
|
User-defined input 6 |
I6 |
– |
I6 |
I6 |
– |
– |
– |
– |
I6 |