Energy Counter Reset
Presentation
The energy counter reset is used to reset the IO module user-defined pulse counters. The energy counter reset order can be activated by:
-
A push-button connected to an IO module digital input, the counters are reset when input is 1.
-
A remote controller or the FDM128 display using the communication network.
-
The IFE or EIFE webpages, only when the IO module is connected to a circuit breaker.
The order issued from a remote controller or the FDM128 display using the communication network corresponds to IO module command. This order requires a communication interface module (IFM, IFE, or EIFE interface).
Input/Output Assignment
The table below lists the possible assignment of the digital inputs according to the predefined application selected on the IO module:
|
Inputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
Energy counter reset: I=1 resets the energy counters |
I4–I6 |
– |
I6 |
I3–I6 |
– |
– |
– |
– |
I1–I6 |