User-Defined Output
Presentation
The user-defined output allows the control of any of the digital outputs. The orders are issued from:
-
A remote controller using a communication network.
-
The IFE or EIFE webpages, only when the IO module is connected to a circuit breaker.
The time response between the order coming from the communication module and the physical activation of the output is greater than 500 ms.
It is possible to force and unforce the output with any type of assignment.
The orders issued from a remote controller using the communication network corresponds to IO module commands. These orders require a communication interface module (IFM, IFE, or EIFE interface).
The user-defined output can be assigned using the EcoStruxure Power Commission software.
The operating mode of the user-defined output is non-latching.
Input/Output Assignment
The table below lists the possible assignment of the digital outputs, according to the predefined application selected on the IO module:
|
Output |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
User-defined output |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |