Energy Reduction Maintenance Setting
Presentation
The energy reduction maintenance setting (ERMS) user-defined application has the same features and generates the same events as the ERMS function of predefined application 3.
Compatible Devices
|
Range |
Minimum Hardware Configuration Required |
|---|---|
|
Fixed or drawout circuit breaker + BCM ULP module with firmware version 4.1.0 and above + MicroLogic P trip unit with firmware version Plogic-2013AN or v8282 and above or MicroLogic H trip unit with firmware version Hlogic-2013AN or v8282 and above. |
Input/Output Assignments
The tables below list the possible assignment of the digital inputs and outputs, according to the predefined application selected on the IO module:
|
Inputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
ERMS OFF order |
I4 |
– |
– |
I4 |
– |
– |
– |
– |
I4 |
|
ERMS ON order |
I5 |
– |
– |
I5 |
– |
– |
– |
– |
I5 |
|
Outputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
ERMS engaged |
O3 |
– |
– |
O3 |
– |
– |
– |
– |
O3 |