Firmware Update
Description
Use the latest version of EcoStruxure Power Commission software for all firmware updates. For more information on IO module firmware versions, refer to Enerlin'X IO Module Firmware Release Note in Related Documents.
| NOTICE |
|---|
|
LOSS OF DATA
Ensure that you take backup of the data log files before
updating the firmware. The data log entries of the IO module may be lost when the IO module
firmware is updated.
Failure to follow these instructions can result in equipment damage.
|
After updating the firmware of one device in the IMU, use the latest version of EcoStruxure Power Commission software to check the firmware compatibility between the IMU devices. The Firmware Update table helps you to diagnose and identify all discrepancy issues between the IMU devices. This table also provides the recommended actions relevant to the detected discrepancies.
Checking the Firmware Version
You can find the firmware version of the devices in the IMU by using EcoStruxure Power Commission software, refer to the EcoStruxure Power Commission Online Help.
Updating the Firmware Using EcoStruxure Power Commission Software
For more information, refer to the EcoStruxure Power Commission Online Help.
The EcoStruxure Power Commission software is available at www.se.com.