User-Defined Alarm Indicator
Presentation
On the ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breakers with MicroLogic 5, 6, or 7 trip units, ten alarms can be assigned to an available digital output for local indication.
The alarm indicator can be configured using the EcoStruxure Power Commission software.
For more information, refer to the following user guides in Related Documents:
-
ComPacT NSX MicroLogic 5/6/7 Trip Units User Guide
-
PowerPacT H-, J-, and L-Frame MicroLogic 5 or 6 Trip Units - User Guide
Compatible Devices
|
Range |
Minimum Hardware Configuration Required |
|---|---|
|
Fixed or withdrawable circuit breaker + MicroLogic 5, 6, or 7 trip unit |
Input/Output Assignment
The table below lists the possible assignment of the digital outputs, according to the predefined application selected on the IO module:
|
Inputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
User-defined alarm 1 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 2 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 3 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 4 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 5 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 6 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 7 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 8 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 9 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
User-defined alarm 10 |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |