Predefined Applications
Introduction
Changing the application rotary switch position does not change the application. After changing the application:
-
the wiring must be checked or changed according to the application.
-
the resources required by user-defined applications must be re-assigned using the EcoStruxure Power Commission software.
WARNING |
|---|
|
DISCREPANCY BETWEEN IO MODULE
WIRING AND APPLICATION
DO NOT change the position of the application rotary switch
during the operation.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Predefined Application Selection Procedure
|
Step |
Action |
LED Status |
|---|---|---|
|
1 |
Rotate the application rotary switch. NOTE: Even though the application rotary switch is rotated,
the selected predefined application is still the same.
|
Input and output LEDs blink: 1 s ON, 1 s OFF. |
|
2 |
Press the test/reset button for 5 to 15 s. The predefined application corresponding to the application rotary switch is selected. |
Input and output LEDs stop blinking. The LEDs indicate the status of the inputs and outputs. |
|
3 |
Check the IO module wiring for the new application. |
- |
|
4 |
Re-assign the resources required by user-defined applications by using the EcoStruxure Power Commission software. |
- |
WARNING