Breaker Status Indicator
Presentation
The following device status can be assigned to the digital outputs for local indication:
-
Position indicator status (OF)
-
Trip indicator status (SD)
NOTE: The trip indicator status is available with ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers. -
Electrical trip indicator status (SDE)
-
Ready to close status (PF)
NOTE: The ready to close (PF) status is available with MasterPacT MTZ, MasterPacT NT/NW, ComPacT NS, and PowerPacT P- and R-frame circuit breakers.
The circuit breaker status can be configured to the IO module digital output for local indication using the EcoStruxure Power Commission software.
Compatible Devices
|
Range |
Minimum Hardware Configuration Required |
|---|---|
|
MasterPacT MTZ circuit breaker |
Fixed or drawout circuit breaker + MicroLogic X control unit + ULP port module |
|
|
|
|
Input/Output Assignment
The following table lists the possible assignment of the digital outputs, according to the predefined application selected on the IO module:
|
Outputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
Position indicator status (OF) |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
Trip indicator status (SD) |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
Electrical trip indicator status (SDE) |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |
|
Ready-to-close status (PF) |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |