DOCA0055EN-09

Digital Inputs

Definition

An IO module has six digital inputs. The digital inputs assigned to a predefined application are pre-configured and cannot be modified.

The remaining available inputs can be configured separately using the EcoStruxure Power Commission software.

Digital Input Types

There are two types of digital inputs:

  • Normal digital inputs, used to record the state of a normally open or normally closed external contact.

  • Pulse digital inputs, used to count pulses delivered by a metering device.

Each digital input can be configured using the EcoStruxure Power Commission software.

NOTE: It is not possible to assign the same function to one of the inputs of IO module 1 and the same input of IO module 2.

Normal Digital Input Parameters

The following parameters can be set with the EcoStruxure Power Commission software. The input signal type must be set to normal.

Description

Setting Range

Factory Settings

Input signal type

  • 0 (Normal digital input)

  • 1 (Pulse digital input)

Normal

Input contact type

  • NO (Normally open contact)

  • NC (Normally closed contact)

NO

Counter threshold

1–4294967294

5000

Digital Input Contact Type

The contact type of the normal digital inputs available for user-defined applications can be configured using the EcoStruxure Power Commission software as:

  • Normally open contact (NO)

  • Normally close contact (NC)

Normal Digital Input Counters

A counter is linked to each normal digital input. The counter is incremented on each rising edge of the linked input.

The digital input counters have the following properties:

  • The counters are saved in non-volatile memory to prevent data loss in case of power loss.

  • The counters can be reset from the IFE or EIFE webpages.

  • The counter stops counting after reaching 4294967294.

  • A threshold is associated to each counter. The counter threshold can be of any value ranging from 1 to 4294967294. The factory setting is 5000.

  • An alarm is generated when a counter reaches the threshold.

  • A digital output can be assigned to any threshold overrun on input counter.

Digital Input Forcing

For maintenance reasons, it is possible to force the state of the digital inputs.

This action can be performed with:

  • FDM121 display

  • EcoStruxure Power Commission software

Digital Input Events

The following events are generated by the digital inputs. For more information on IO module events, refer to Events and Alarms.

Code IO1

Code IO2

Description

Type

Priority

Reset

1555 (0x0613)

1811 (0x0713)

Input 1 rising edge (NO contact) or falling edge (NC contact)

Event

NA

NA

1556 (0x0614)

1812 (0x0714)

Input 2 rising edge (NO contact) or falling edge (NC contact)

Event

NA

NA

1557 (0x0615)

1813 (0x0715)

Input 3 rising edge (NO contact) or falling edge (NC contact)

Event

NA

NA

1558 (0x0616)

1814 (0x0716)

Input 4 rising edge (NO contact) or falling edge (NC contact)

Event

NA

NA

1559 (0x0617)

1815 (0x0717)

Input 5 rising edge (NO contact) or falling edge (NC contact)

Event

NA

NA

1560 (0x0618)

1816 (0x0718)

Input 6 rising edge (NO contact) or falling edge (NC contact)

Event

NA

NA

1561 (0x0619)

1817 (0x0719)

Threshold overrun on input 1 counter

Alarm

Medium

Manual or remote

1562 (0x061A)

1818 (0x071A)

Threshold overrun on input 2 counter

Alarm

Medium

Manual or remote

1563 (0x061B)

1819 (0x071B)

Threshold overrun on input 3 counter

Alarm

Medium

Manual or remote

1564 (0x061C)

1820 (0x071C)

Threshold overrun on input 4 counter

Alarm

Medium

Manual or remote

1565 (0x061D)

1821 (0x071D)

Threshold overrun on input 5 counter

Alarm

Medium

Manual or remote

1566 (0x061E)

1822 (0x071E)

Threshold overrun on input 6 counter

Alarm

Medium

Manual or remote

1570 (0x0622)

1826 (0x0722)

Input 1 not forced or forced change

Event

NA

NA

1571 (0x0623)

1827 (0x0723)

Input 2 not forced or forced change

Event

NA

NA

1572 (0x0624)

1828 (0x0724)

Input 3 not forced or forced change

Event

NA

NA

1573 (0x0625)

1829 (0x0725)

Input 4 not forced or forced change

Event

NA

NA

1574 (0x0626)

1830 (0x0726)

Input 5 not forced or forced change

Event

NA

NA

1575 (0x0627)

1831 (0x0727)

Input 6 not forced or forced change

Event

NA

NA

Pulse Input

The maximum number of allowed user-defined pulse inputs are six, with one or two IO modules. All the inputs can be configured as a pulse input using the EcoStruxure Power Commission software. Also, the pulse rate, pulse polarity, and the pulse unit can be configured using the EcoStruxure Power Commission software. A pulse counter is activated when the corresponding digital input of IO module 1 or IO module 2 is configured as a pulse input.

For example, if I2 on IO module 1 is set as a pulse input, I2 on IO module 2 cannot be set as a pulse input. If I3 on IO module 2 is set as a pulse input, I3 on IO module 1 cannot be set as a pulse input.

The minimum pulse width is 40 ms.

Pulse Digital Input Parameters

The following parameters can be set with the EcoStruxure Power Commission software. The input signal type must be set to pulse.

Description

Setting Range

Factory Settings

Input signal type

  • Normal

  • Pulse

Normal

Pulse polarity

  • Low to high (rising edge of the pulse)

  • High to low (falling edge of the pulse)

Low to high

Pulse unit

  • Active energy: Wh

  • Reactive energy: VARh

  • Apparent energy: VAh

  • Volume: cubic-meter

Wh

Pulse weight

0 to 16777215

1

The pulse weight must be calculated according to the characteristics of the pulses delivered by the meter.

Examples:

  • If each pulse delivered by an active energy meter corresponds to 10 KWh, and the pulse unit is set to Wh, the pulse weight must be set to 10,000 (Wh).

  • If each pulse delivered by a volume meter corresponds to 125 liters, and the pulse unit is set to m3, the pulse weight must be set to 0.125 m3.

  • If each pulse delivered by a volume meter corresponds to 1 gallon, and the pulse unit is set to m3, the pulse weight must be set to 0.003785 m3.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.