DOCA0055EN-09

Application 9: Custom

Presentation

The custom application is used to perform user-defined applications with the IO modules.

The user-defined applications performed by the IO modules require prior configuration using the EcoStruxure Power Commission software.

User-Defined Applications

The user-defined applications are categorized according to:

  • Protection functions

  • Control functions

  • Energy management functions

  • Monitoring functions

Each user-defined application is described in IO Module User-Defined Applications.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?