Troubleshooting
|
Symptoms |
Cause |
Action |
|---|---|---|
|
Cradle management application is enabled and it is not working as expected |
EIFE is connected in IMU |
|
|
IO module applications are not working as expected |
Application is not validated |
|
|
System configuration is not correct |
|
|
|
ULP wiring is not correct |
|
|
|
Digital input and digital output wiring is not correct |
Force the state of the input and output with the EcoStruxure Power Commission software to check the wiring. |
|
|
Digital output is not working |
Wiring issue |
|
|
Configuration issue |
|
|
|
Digital output is damaged |
|
|
|
Digital input is not working |
Wiring issue |
|
|
Configuration issue |
|
|
|
IO module is in degraded mode, according to the ULP LED |
Configuration file transfer aborted from the EcoStruxure Power Commission software |
Reload the configuration file with the correct assignments |
|
IO module is in configuration discrepancy mode, according to the ULP LED |
Duplicate assignments within the same IO module |
Check the application assignments with the EcoStruxure Power Commission software |
|
Duplicate predefined application 1 to 8 across the two IO modules |
Modify the predefined application assigned to one of the IO modules |
|
|
Duplicate input/output assignments across the two IO modules |
Check the input/output assignments with the EcoStruxure Power Commission software |
|
|
Cradle management and drawer management applications are configured together |
Configure only one of the applications, cradle management, and drawer management, with the EcoStruxure Power Commission software |
|
|
Switching on to ERMS mode is not possible |
Discrepancy with ERMS order alarm is active |
Reset the alarm |
|
Inconsistency of the ERMS setting |
Check and modify the ERMS setting |
|
|
Switching off the ERMS mode is not possible |
Discrepancy with ERMS order alarm is active |
Reset the alarm |
|
Inconsistency of the ERMS setting |
Check and modify the ERMS setting |
|
|
Closing the circuit breaker is not possible either locally or remotely |
Inhibit close order is activated by the IO module |
Enable the close order from the IO module. |
|
Inhibit close order is activated by a remote controller using the communication network |
Enable the close order from the remote controller. |