Application 3: Cradle Management and Energy Reduction Maintenance Setting
Presentation
Application 3 is the combination of two functions:
-
The cradle management function, with the same features as the predefined application 1.
-
The energy reduction maintenance setting function described here in detail.
Energy Reduction Maintenance Setting Function
The energy reduction maintenance setting (ERMS) function is compatible only with the MasterPacT NT/NWand ComPacT NS or PowerPacT P- and R-frame circuit breakers. It allows the selection of the MicroLogic P and H trip unit settings: Normal and ERMS mode.
This application is used to reduce the instantaneous (Ii) protection settings in order to trip as fast as possible when a fault occurs. The factory setting for Ii protection in ERMS mode is 2xIn. This protection parameter can be modified using the EcoStruxure Power Commission software.
The ERMS mode is in the OFF state if the Ii setting is less than the ERMS setting.
DANGER |
|---|
|
HAZARD OF ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
If any of the basic protection settings using the rotary dial is modified on the MicroLogic trip unit while in ERMS mode, the MicroLogic trip unit switches immediately to the normal mode. The MicroLogic trip unit returns automatically to the ERMS mode after 5 seconds.
The selection of the normal or ERMS mode is made by a selector switch connected to two inputs. When the ERMS mode is engaged, ERMS is displayed on the display of the MicroLogic trip unit and a pilot light connected to output O3 is in the ON state.
The locking pad of the communication interface module (IFM or IFE interface) must be in the UNLOCK position (padlock open) while performing the energy reduction maintenance setting (ERMS).
The parameter ACCESS PERMIT in the COM setup or Remote setting menu on the display of the MicroLogic trip unit must be set on YES for IMU without IFM or IFE interface.
This is based on the following behavior:
-
IMU with IFM or IFE interface
-
Setting access permit parameter:
The access permit parameter can be changed only from IFM or IFE interface using the LOCK/UNLOCK dial.
-
Behavior:
ERMS ON and OFF orders are executed even if the access permit parameter is set as NO.
-
-
IMU without IFM or IFE interface
-
Setting access permit parameter:
The access permit parameter can be changed only from the display of the MicroLogic trip unit.
-
Behavior:
ERMS ON and OFF orders are not executed if the access permit parameter is set as NO.
-
For more information, refer to the following user guides in Related Documents:
- MicroLogic P Trip Units - User Guide
- MicroLogic H Trip Units - User Guide
Compatible Devices
|
Range |
Minimum Hardware Configuration Required |
|---|---|
|
Fixed or drawout circuit breaker + BCM ULP module with firmware version 4.1.0 and above + MicroLogic P trip unit with firmware version Plogic-2013AN or v8282 and above or MicroLogic H trip unit with firmware version Hlogic-2013AN or v8282 and above |
Input/Output Assignment
|
Input |
Assignment |
|---|---|
|
I1 |
Cradle connected position contact (CE) |
|
I2 |
Cradle disconnected position contact (CD) |
|
I3 |
Cradle test position contact (CT) |
|
I4 |
Energy reduction maintenance setting OFF order |
|
I5 |
Energy reduction maintenance setting ON order |
|
I6 |
Available NOTE: The outputs can be assigned to the cradle position status with the EcoStruxure Power Commission software. For more
information, refer to the user-defined applications.
|
|
Output |
Assignment |
|---|---|
|
O1, O2 |
Available NOTE: The outputs can be assigned to the cradle position status with the EcoStruxure Power Commission software. For more
information, refer to the user-defined applications.
|
|
O3 |
Energy reduction maintenance setting engaged |
Wiring Diagram
ERMS Mode Engaged
A digital output is assigned to indicate that the ERMS mode is engaged. This output relay is closed in the ERMS mode.
|
ERMS may be activated after a short delay due to internal controls in the system. Ensure that the output 3 (O3) of IO module is ON, and MicroLogic HMI displays ERMS before operating the equipment. |
Cradle Management Events
The events generated by the cradle management function are the same as the events generated by the Application 1.
ERMS Events
The following alarm is generated by the ERMS function. For more information on IO module events, refer to Events and Alarms.
|
Code |
Description |
Type |
Priority |
Reset |
|---|---|---|---|---|
|
3072 (0x0C00) |
Discrepancy with ERMS orders |
Alarm |
Medium |
Manual or remote |
|
3073 (0x0C01) |
ERMS setting inconsistency |
Alarm |
High |
Auto |
|
3074 (0x0C02) |
ERMS engaged for more than 24 hours |
Alarm |
High |
Auto |
Discrepancy with ERMS Orders
The IO module detects the ERMS order discrepancy and generates an alarm when I4 and I5 are 1 or when I4 and I5 are 0.
When the alarm is generated while ERMS mode is engaged, it is necessary to reset the alarm in order to switch off the ERMS mode.
When the alarm is generated while ERMS mode is not engaged, it is necessary to reset the alarm in order to switch on the ERMS mode.
Recommended action: Check wiring from the circuit breaker to the IO module and the inputs of the IO module.
ERMS Setting Inconsistency
This event is generated in ERMS mode when the ERMS setting (Ierms) is set above the Ii protection setting of trip unit.
Recommended action: Check the ERMS setting (Ierms).
ERMS Engaged for More Than 24 Hours
A maintenance operation requiring switching the Ii protection settings in ERMS mode normally lasts for no more than a few hours. Therefore, when the ERMS mode is engaged for more than 24 hours, an event is generated to remind you to switch the Ii protection settings back in normal mode.
Recommended action: Disengage ERMS by selector switch.
DANGER