Cradle Management
Presentation
The cradle management application is performed by the predefined application 1. In addition, the user-defined application allows the assignment of the cradle position to available digital outputs for local indication.
-
The cradle and the drawer applications cannot be configured together.
-
The cradle management application for MasterPacT MTZ circuit breakers is performed by the EIFE interface, not by the IO module. For more information, refer to the EIFE Embedded Ethernet Interface User Guide.
Compatible Devices
|
Range |
Minimum Hardware Configuration Required |
|---|---|
|
|
|
|
Input/Output Assignment
The tables below list the possible assignment of the digital inputs and outputs, according to the predefined application selected in the IO module:
|
Inputs |
Predefined Application Selected |
|||||||||
|---|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 (IO1) |
9 (IO2) |
|
|
Cradle connected position contact (CE) |
I1 |
– |
I1 |
– |
– |
– |
– |
– |
– |
I1 |
|
Cradle disconnected position contact (CD) |
I2 |
– |
I2 |
– |
– |
– |
– |
– |
– |
I2 |
|
Cradle test position contact (CT) |
I3 |
– |
I3 |
– |
– |
– |
– |
– |
– |
I3 |
-
The cradle test position contact is not applicable.
-
I3 must be always wired to have I3=1.
|
Outputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
Cradle connected position status |
O1, O2, O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1, O2, O3 |
|
Cradle disconnected position status |
O1, O2, O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1, O2, O3 |
|
Cradle test position status |
O1, O2, O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1, O2, O3 |