Alarm Indicators
Presentation
Alarms can be assigned to an available digital output for local indication on:
-
MasterPacT MTZ circuit breaker with MicroLogic X control unit
-
MasterPacT NT/NW, ComPacT NS, or PowerPacT P- and R-frame circuit breaker with MicroLogic A/E/P/H trip unit
The alarm that can be assigned to a digital output depends on the MicroLogic trip unit. The alarm indicator can be configured using the EcoStruxure Power Commission software.
|
Alarm |
Compatible MicroLogic X Control Units |
Compatible MicroLogic A/E/P/H Trip Units |
|
|---|---|---|---|
|
Ground fault alarm |
MicroLogic 2.0 X, 3.0 X, 5.0 X, and 6.0 X |
MicroLogic 6 A/E/P/H |
|
|
Earth-leakage alarm |
MicroLogic 7.0 X |
MicroLogic 7 A/P/H |
|
For more information, refer to the following user guides in Related Documents:
- MasterPacT MTZ MicroLogic X Control Unit - User Guide
- MicroLogic A and E Trip Units - User Guide
- MicroLogic P Trip Units - User Guide
- MicroLogic H Trip Units - User Guide
Compatible Devices
|
Range |
Minimum Hardware Configuration Required |
|---|---|
|
MasterPacT MTZ circuit breaker |
Fixed or withdrawable circuit breaker + MicroLogic X control unit with Ground fault alarm Digital Module installed + ULP port module |
|
Fixed or withdrawable circuit breaker + MicroLogic A/E/P/H trip unit + BCM ULP module with firmware version 4.1.0 and above |
Input/Output Assignment
The table below lists the possible assignment of the digital outputs, according to the predefined application selected on the IO module:
|
Inputs |
Predefined Application Selected |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
|
Alarm |
O1–O3 |
O3 |
O1, O2 |
O3 |
– |
– |
– |
– |
O1–O3 |