About the device
The Schneider Charge when installed with Anti-Tripping Module, provides an end-to-end solution for power load management. For more information, refer Anti-tripping System.
Operating elements
|
A |
Cable winding trough |
When not in use, wrap the charging cable around the charging station’s trough to avoid tripping hazards and equipment damage. |
|
B |
Front indicator light |
Indicates the status of the charging station and charging session. Refer LED Indication. |
|
C |
Side indicator light |
Indicates status during Wi-Fi® access point commissioning and anti-tripping module pairing. |
|
D |
Functional button (Push button) |
Press to enable Wi-Fi access point/Reset PIN Code/anti-tripping module pairing (power off and then back on the product to enable this button). |
|
E |
Charging socket |
Plug in your T2 charging cable. |
-
Anti-tripping module is designed for use with the Schneider Charge. Do not use with other electrical devices.
-
When the Anti-tripping module is employed with Schneider Charge as a standalone, the use of PowerTag in the system is precluded, thereby restricting the functionality of certain features such as Reduce My Bill - AI.