DUG_Schneider Charge_WHP-01

Enabling charging authorisation

You can establish an authorisation process every time a charger is connected to an EV, Wiser Home app will ask for your authorisation prior to initiating the charging process to prevent anyone to use the charger without authorisation.
NOTE: If charging authorisation is not enabled, the charging will start immediately upon connecting the charger to an EV.
  1. On the Home page, tap All > Schneider Charge > Device details.
  2. Turn on the toggle switch (A) to enable charging authorisation.
When enabled, upon connecting the charger to an EV, tap Authorise charge (B) in the control panel to initiate the charging process.
If authorisation is not approved control panel displays an alert banner that charger is currently not authorised to charge your EV.
TIP: On the home screen, you can tap Unlock to initiate the charging process.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?