DUG_Schneider Charge_WHP-01

Creating a schedule

The Schneider Charge can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
  1. On the Home page, tap All > Schneider Charge.
  2. Tap Charging Mode.
    NOTE: If you have Schneider Charge installed with Wiser Hub 2nd generation you can also navigate the following path to create schedules:
    • On the Home page, tap .

    • Tap Schedules > EV schedule. Proceed with step 3.

  3. On the EV Charging Mode page, select Customized Schedule.
    NOTE: The Schneider Charge will have a default schedule pre set to the user. You can edit the schedule as required.
    IMPORTANT: It is required to set the on and off state for a schedule.
  4. Select days (A).
  5. Tap (B) to edit the schedule.
  6. Select a state (On/Off) (C), time period (D) and tap Set.
    TIP:
    • You can add multiple schedules based on your requirement. Select days (A), tap (E), set on/off state and time.

    • You can copy the existing schedule to the days of your choice. Tap (F), select the days and tap Copy.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?