Pairing Anti-Tripping Module with Schneider Charge
-
Make sure the installation of Anti-Tripping Module and Schneider Charge is complete according to the installation manual.
-
Do not shut down the power supply during pairing process.
Activate pairing mode
-
Activate pairing mode in Anti-Tripping Module as mentioned below:
-
For EVAxHPC1 module:
Power On the module and then press COM button for 5 s to enter the pairing mode.
All LEDs blinks green. -
For EVA2HPC3 module:
Using a screw driver set the first and last DIP switch to ON position and then Power On the module.
Only System LED blinks green.
-
-
Power On the Schneider Charge. When the side LED turns green, press the Push button on Schneider Charge 3 times to activate the pairing mode.
Side LED blinks blue.
When both are in pairing mode, wait for a few minutes for them to connect with each other.
Upon successful pairing:
-
On EVAxHPC1 module, both Peak LED and Run LED turn solid green.
-
On EVA2HPC3 module, System LED blinks green while Communication LED turn solid green.
-
On Schneider Charge, side LED turn solid green.
Unpairing / Aborting from pairing mode
Enter pairing mode as mentioned above and follow below procedure to unpair or abort pairing mode:
-
On EVAxHPC1 module, before successful pairing press COM button once to abort.
-
On EVA2HPC3 module, set other current rating before successful pairing using DIP switch.
-
On Schneider Charge, press the side button 5 seconds to abort.